AXIS#.CLRFAULTS
Description
When AXIS#.CLRFAULTS is sent, the axis will try to clear all active faults on the axis. When a fault occurs, the fault is registered in the drive fault handler. AXIS#.CLRFAULTS clears the fault from the drive fault handler. However, if the fault still exists in the system, AXIS#.CLRFAULTS fails and the fault is re-registered in the fault handler.
If the AXIS#.CLRFAULTS succeeds, then the reply to AXIS#.FAULTS states that no faults exist. If the condition that triggered the fault is still present, the fault condition will remain.
See Faults and Warning Messages for details regarding the behavior of individual faults.
Note that executing an axis disable (AXIS#.DIS ) followed by a axis enable (AXIS#.EN ) has the same effect as executing AXIS#.CLRFAULTS.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Command |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported
Related Topics